Browse FAQs

What is the pinout to connect TWIDO CANopen Master module (TWDNC01M) to an Altivar drive 31 ?

Published date: 29 June 2020

The pinout to connect the DB9 connector on the TWIDO CANopen module (TWDNC01M) to a ATV 31 drive is given below:
TWDNC01M (DB9) ------------------------------------------>>> ATV 31 (RJ 45 )

CAN_H ( 7 ) ------------------------------------------>>> CAN_H ( 1 )

CAN_L ( 2 ) ------------------------------------------>>> CAN_L ( 2 )

GND ( 3 ) ------------------------------------------>>> GND ( 3 )


Legacy KB System (APS) Data: RESL182258 V1.0, Originally authored by TVe on 02/21/2007, Last Edited by TVe on 02/21/2007
Related ranges: Twido

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.