Browse FAQs

What could cause the error "Error during Connect (This isn't a valid PLC address, or PLC is busy, or Media is off.)" when trying to connect to the Unity Pro simulator?

Published date: 17 June 2020

One possible explanation for this error is a conflict between Unity and the v6.0 Ethernet MBX driver. Uninstalling the v6.0 Ethernet MBX driver and rebooting the PC will correct the issue.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.