Browse FAQs

Can a literal value be used as an input in an SEL block?

Published date: 13 May 2020

The IN0, IN1 inputs and OUT output must be identical datatypes. However, if you link the output (OUT) of the SEL block to the input of another block, you can then configure literal values as inputs on IN0 and IN1.


Legacy KB System (APS) Data: RESL183349 V1.0, Originally authored by DaSo on 04/06/2007, Last Edited by DaSo on 04/06/2007
Related ranges: Concept

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.