Browse FAQs

What is the syntax of the IN Parameter of the ADDM block when using the DATA_EXCH block to communicate to a Modbus device through a TSXETG100.

Published date: 26 June 2020

Goals and Symptoms

Communication with M340, DATA_EXCH, & TSXETG100

Facts and Changes

A minimum version of Unity Pro v4.0 and a M340 CPU or NOE v2.0 must be used for the DATA_EXCH to work properly.

Causes and Fixes

The syntax of the IN Parameter of the ADDM block when using the DATA_EXCH block to communicate to a Modbus device through a TSXETG100 is displayed in the screen shot below.


The breakdown of the IN string 'Ethernet_1{192.168.10.22}3.TCP.MBS' is as follows:

Ethernet_1 - Name of the Ethernet Network interface on M340 to send request out
{192.168.10.22} - The IP address of the TSXETG100 ModbusTCP to Modbus bridge
3.TCP.MBS - the 3 is the Modbus address and the TCP.MBS specifies using a Modbus TCP request

NOTE- For more information on using the DATA_EXCH function with M340 reference Resolution Number: 197874



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.