Browse FAQs

Concept 2.6. Trying to assign an address to a variable using the format '%I1' produces error message: "Invalid selector of register address Error ID: NCC-19902".

Published date: 10 February 2020

Open the Concept project and navigate to Options - Preferences and choose IEC format. Once this option is chosen,
the following rule applies:

Entering %0x0001 on a pin will display %Q0001 on the block.
Entering %1x0001 on a pin will display %I0001 on the block.
Entering %3x0001 on a pin/block will display %IW0001 on the block.
Entering %4x0001 on a pin/block will display %QW0001 on the block.

You will find that this will alter the \windows\concept.ini file' [Common] section. AddrStyle=3 will be set.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.