Browse FAQs

How to uninstall TwidoSuite when it doesn't show up in "Add or Remove Programs"?

Published date: 30 June 2020

If TwidoSuite is not in the "Add or Remove Programs" first verify that you have administrative rights on the PC. Then go to the registry and look under;
HKEY_LOCAL_MACHINE
HKEY_LOCAL_MACHINE\SOFTWARE
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\TwidoSuite

Once you find this folder and delete it, reboot the PC and then go back and search again on the PC and remove
anything that says TwidoSuite except for the programs.


Note:  Twido and TwidoSuite became obsolete 12/31/16 and has been replaced with the M221 and Ecostruxure Machine Expert Basic ( formally SoMachine Basic), The Twido program can be imported into Ecostruxure Machine Expert Basic.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.