Browse FAQs

Can I use the TCSMCNAM3MOO2P cable to program a Twido?

Published date: 01 July 2020

Issue:
Can the TCSMCNAM3MOO2P be used to program the Twido controller?

Product Line:
All Twido controllers

Cause:
Incorrect cable and it will not work.

Resolution:
No. The TCSMCNAM3MOO2P cable has a USB on one end and a RJ45 on the other end. The Twido has a mini-din connector on its end. The cable is used for Altistart 22, Altivar 312, and Lexium 32i.


Note: the Twido has been replaced by the M221 product line for more information on this contact your local distributor or Schneider Electric sales office.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.