Browse FAQs

Is Concept programming software supported on Windows 7?

Published date: 09 April 2020

Issue:
Can you running Concept on Windows 7 will it work?

Product Line:
All PLC that can run on Concept software

Environment:
Concept software last release 2.6 SR7


Cause:
Trying to install on a Windows 7 64 bit machine.

Resolution:
Concept 2.6 SR7 is supported on Windows 7 Professional 32-Bit. Windows 7 64 Bit is not supported. Concept will not run on Windows 10 either if you can not upgrade it is recommended to install on  a VM with XP.
Concept is obsolete and there will be no updates to the software. The recommendation is to upgrade to the Ecostruxure Control Expert and upgrade system.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.