Browse FAQs

Which EM4800 Current Transformers (CT's) require shorting blocks?

Published date: 23 May 2020

Issue
Need to know which EM4800 CTs need shorting blocks. 
 
Product Line
E(M)4800
 
Environment
Installation of the shorting block with EM4800 CT's.
 
Resolution
When using 80 mA CTs or 5 A CT's, shorting blocks are recommended. 333 mV CT's do not require shorting blocks because they have a burden resistor built into the CT that limits the output voltage to 333 mV under all conditions. 

NOTE: If a 1/3 V CT was shorted, the internal burden resistor and the CT would be shorted at the same time. This would effectively be the same as shorting a current secondary CT and would cause no harm, despite the fact that it is not needed.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.