Browse FAQs

How can different metered quantities from different device types be displayed on the same table in System Manager Software?

Published date: 14 May 2020

Product Line  
SMS 3.3.x
SMS 4.x

Resolution
SMS (System Manager Software) does not support assigning different metered quantities from different device types on the same table. For example: Displaying A phase current from a CM3000 and B phase current from a PM800. The work-around is to create a GFX (Interactive Graphics) diagram with a value block for each device and quantity.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.