Browse FAQs

Why columns do not line up in an Excel spreadsheet when a report is exported from Tenant Metering Software v1.0.1?

Published date: 14 May 2020

Product Line            
TMS 1.0.1

Resolution
Placement of commas are very important when exporting reports in Tenant Metering Software (TMS) v 1.0.1 as a .CSV file. Commas are used to separate the data fields. If an account contains commas then the columns will not line up when Export to File is selected. If a row of the spreadsheet is not lining up correctly Edit the Account and remove any commas. When you generate the bill again the columns will line up.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.