Browse FAQs

Is it possible to acquire Power Quality Data from ION Meters using Modbus?

Published date: 29 May 2020

Issue
User would like to acquire Power Quality Data from ION Meters via Modbus communications

Product Line
ION Meters

Environment
Modbus communication

Resolution
Although it is possible to acquire power quality data from ION meters when using the Modbus protocol, the procedure is not supported by Technical Support.

Basic quantities and associated Modbus registers are documented in the Modbus register map. For the Modbus register map and additional information on using the Modbus protocol with ION meters, please refer to FA300088.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.