Browse FAQs

System Manager Software (SMS) v 3.3.x.x or v 4.xx on Windows XP Professional 64-bit, Windows Server 2003 64-bit, or Windows 2008 Operating Systems?

Published date: 14 May 2020

Product Line   
SMS 3.3.x
SMS 4.x

Resolution
SMS is not supported on a 64 bit OS.

  • SMS version 3.3.x.x may install, but is not supported.
  • System Manager Software (SMS) version 4.x will not install on a Windows 64-bit Operating System (OS).

SMS, however, can be run within a virtual machine with a supported OS where that virtual machine is hosted by a 64 bit OS.

Support is provided for the SMS install only. Licensing to support the VM will be the responsibility of the user. The creation and deployment of the VM and the VM environment are also the responsibility of the user.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.