Browse FAQs

What is the Comtrade Format for System Manager Software (SMS) Waveform Captures?

Published date: 19 May 2020

Product Line 
SMS 3.3.x
SMS 4.x

Resolution
A Comtrade file is actually made up of two different files, a *.cfg and a *.dat. The *.cfg file is in ASCII format, while the *.dat file is in binary format. Both of these files are required to make a single Comtrade file.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.