Browse FAQs

ION meters: what is the maximum character length allowed for the formula register of the arithmetic module?

Published date: 29 May 2020

The arithmetic module can support a formula that has up to 50 characters.
This is coded into the device's firmware/ION Enterprise and it is not configurable. If attempting to input a formula longer than 50 characters an "Operation Incomplete" window will appear with a "Formula too long" message.


Legacy KB System (APS) Data: RESL201650 V1.0, Originally authored by DaMi on 03/16/2010, Last Edited by DaMi on 03/16/2010
Related ranges: ION7300, ION8800, ION8600, ION7550/ION7650

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.