Browse FAQs

Information Manager reports show default graphs when viewed through the SMS Webclient.

Published date: 19 May 2020

Issue
When trying to view a graph created by Information Manager in the Webclient for some reason the Webclient graph does not match the one in Information Manager. The Webclient just displays a default graph which effects trends, bar charts, and pie charts. The screen shoots below show an example of the issue.

If the report is viewed from Information Manager it appears as follows.


However when the report is viewed through the webclient it appears as follows.


Product Line
SMS 3.3.x
SMS 4.x
 

Resolution
The fix is to create a Mime Type for the .peg extension. The .peg file is the file within Information Manager reports that contains the graph information.

Creating a Mime Type for a Windows 2003 Server:
1.) Go to Administrative Tools > Internet Information Services Manger
2.) Right Click on the computer name and then select properties
3.) Click the MIME Types... button
4.) Click new
5.) enter the extension .peg in the Extension: field and MIME type should be image/peg.

6.) IISRESET

The report graphs should now show properly within the Webclient.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.