Browse FAQs

ION8500 Firmware for V281, V265, V262 and V244

Published date: 19 May 2020

Product Line  
ION8500

Resolution

When upgrading your meter's firmware please download the latest firmware version (.upg file) and the equivalent Meter Template (.dcf file).

You can upgrade meter firmware using ION Setup or ION Enterprise. See the "Upgrading ION Device Firmware" technical notefor complete details.

Important Device Update (Jan 2008)

To discover whether your meter is a revision A or revision B meter, check the faceplate on the meter.

Revision B (RevB) meters will have a "RevB" written on the right hand side of the label, above the serial number. RevA meters will not have this mark on the label.

To upgrade a RevB device, users must use the latest ION Setup.

 

Firmware for Revison A meters
 

Firmware (.UPG file) text text RMICAN Approved
Low Current
(Class 2)
Standard
(Class 20)
ECR
(Class 2-20)
 
8500V2658500V265.exe  
8500V2628500V262_8000_FAC_V1.1.0.exe RMICAN Approved
V244 9S-39S8500_9S_39S_1A.exe

V244 35S8500_35S_1A.exe

V244 36S-76S8500_36S_76S_1A.exe

V244 9S-39S8500_9S_39S_5A.exe

V244 35S8500_35S_5A.exe

V244 36S-76S8500_36S_76S_5A.exe

V244 9S-39S8500_9S_39S_ECR.exe

V244 35S8500_35S_ECR.exe

V244 36S-76S8500_36S_76S_ECR.exe

 

Firmware for Revison B meters


8500V2818500V281.exe

text
text
text
text


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.