Browse FAQs

ION8500 Meter Template Files

Published date: 20 May 2020

Product Line
ION8500

Environment
Templates

Resolution
You can install meter templates using ION Setup. See the "Upgrading ION Device Firmware" technical note for complete details.

Install Templates with ION Setup

  1. Download the device template and save it to your ION Setup TEMPLATE folder (select the file below that matches your meter's feature set).

Use these .DCF files with ION Setup to perform firmware upgrades. These are default meter templates only. If you have custom programming in your meter, create your own template file before performing the firmware upgrade.

  1. Follow the upgrade procedures outlined in the Upgrading ION Device Firmware technical note.
See the .zip below for the following templates:
Version Low Current (Class 2) Standard (Class 20) ECR (Class 2-20)
V264-265 8500_FAC-9S-39S-36S-76S_V2.6.0.0.9
8500_FAC-35S_V2.6.0.0.9
   
V262 8500_FAC-9S-39S-36S-76S_V2.6.0.0.2
8500_FAC-9S-39S-36S-76S_V2.6.0.0.2
   
V244 8500_v240_FAC-9S-39S_V1.9.0.0.0
8500_v240_FAC-35S_V1.9.0.0.0
8500_v240_FAC-36S-76S_V1.9.0.0.0
text8500_v240_FAC-C2A-9S-39S_V1.9.0.0.0
8500_v240_FAC-C2A-35S_V1.9.0.0.0
8500_v240_FAC-C2A-36S-76S_V1.9.0.0.0

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.