Browse FAQs

Connection Schedule completed but Site Connection did not complete message

Published date: 02 June 2020

Issue
The message "site connection schedule completed, but site connection did not complete" may appear in the schedule event log.

Product line
ION Enterprise
StruxureWare Power Monitoring (SPM) 7.0.x
Power Monitoring Expert 7.2.x, 8.x

Causes

The connection for the referenced site did NOT end for one of the following reasons:

  • all records were uploaded
  • the maximum time alloted for a site expired
    i.e.: connection terminated prematurely due to end of schedule
Resolution

There is no one solution. Determine if onboard logs are all uploaded using the diagnotic viewer 
Management console -> Tools -> System -> Diagnostic viewer
If all onboard logs are not uploaded perhaps increase the connection time in the schedule.
Alternatly determine why logs could not be uploaded in the alloted time period. Bad communictions? timeouts?

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.