Browse FAQs

What Modbus address or word shows you motor speed in rpm's on the ATV61 and ATV71 Drives?

Published date: 19 June 2020

Issue:
ATV61/71 Modbus address or word that shows you motor speed in rpm

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
4X modbus address word showing rpm's motor speed.

Resolution:
rFrd= Output speed in rpm's modbus address 8604
rFr= Output frequency in hz modbus address 3202
Please note you might have an offset when reading the modbus addresses.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.