Browse FAQs

What is the maximum number of Active Connections allowed on an EGX100 Gateway and can it be changed?

Published date: 19 May 2020

Issue
What is the maximum number of Active Connections allowed on an EGX100 Gateway and can it be changed?

Product Line
EGX100

Environment
Active Connections

Resolution
The default number of Active connections allowed on an EGX100 Gateway is 32 Modbus/TCP Server Connections. This value can be changed to up to 48 connections with Firmware 2.7 up to 2.9 inclusive.
This can be done by connecting to the Gateway's web page and then adding /AdvCommsSetup.htm to the address of the gateway. This will bring you to the Advanced setup page for communications.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.