Browse FAQs

MET1482 8-Temperature Sensor Module Installation Sheet, Instruction Bulletin (ANSI), 63230-216-243A1, May 2007

Published date: 19 May 2020

The MET1482 module can connect eight temperature APS_SENSORS (RTDs) of the same type:
Pt100, Ni100, or Ni120 type RTDs, according to parameter setting
Three-wire temperature APS_SENSORS
The temperature measurement provides for thermal overload and temperature monitoring.


see attachment:

63230-216-243_MET1482_InstallSheet.pdf


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.