Browse FAQs

Calculating the pulse weight in WAGES Device configuration utility (Devcon).

Published date: 19 May 2020

The "pulse weight" must be calculated based on the units that are being selected. Example: Using a gas transducer that has a flow rate of 1 pulse per 1000 cubic feet. Assuming that 100 cubic feet equals one Therm, then the actual pulse weight would be 10 Therms per pulse (1000 cubic feet / 100 cubic feet per therm = 10). The "Units" is only a label that will be displayed on the System Manager Software WAGES Report or Table.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.