Browse FAQs

What is the cable wire size and insulation type on the BCM42-SC 50 amp split core Current Transformer (CT)?

Published date: 19 May 2020

Issue
Cable wire size and insulation type for the BCM42-SC 50 amp Split Core Current Transformer (CT)

Product Line
BCM42-SC

Environment
Wiring 

Resolution
The BCM42-SC (Branch Current Monitor with Split core CTs) comes with 50 amp split core CT's. The leads on the CT are 22 AWG with type THHN insulation. The leads are not plenum rated.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.