Browse FAQs

Missing CMDVF and CMDLC document number 63230-305-200.

Published date: 19 May 2020

The Series 3000, 4000 Circuit Monitor Instruction Bulletins refer to document 63230-305-200 for information on the displays. The two displays supported are the Circuit Monitor Display Vacuum Florescent (CMDVF) and the Circuit Monitor Display Liquid Crystal (CMDLC). This document was never release so refer to document 63230-305-29 or each meters instruction bulletin for dimensional information on the display and mounting.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.