Browse FAQs

Error 16 in Advanced Reports when creating or editing a report. You do not have the right to “Add objects to the folder” or "Edit objects".

Published date: 20 May 2020

Issue

SMS user levels 2 5 go through creating the report and when pressing Finish at the final step get an Error 16 with message that they dont have the rights to Add objects to the folder.
Summary

The default SMSPE 4.0 Operator account has an security level of 5. So the user is part of the SMS AR Operators group in CE (SMSPE levels 2-5 map to this group). This group has view on demand rights (see rights on PowerLogic Reports folder). However this group does not have rights to add objects to that folder. Therefore, when the user attempts to create/edit a report they will get an error when clicking Finish on the final step of the wizard. The resolution is to change the Access Level in Advanced Reports, Crystal Management Console for the "SMS AR Operators" to allow the user to Edit and Create objects to folders.

Symptoms

Error publishing new report (report name), you do not have the right to 'Add objects to the folder' (id -1) fc "table' (id -215). Please contact your system or permissions administrator if you require this right.

Error publishing new report (report name), you do not have the right to 'Edit objects' (id -6) for 'report name' (50526). Please contact your system or permissions administrator if you require this right.


Cause
The cause is that System Manager Software (SMSPE) 4.0 users, with security Level 2 - 5, do not have permissions to the folders.

Resolution

Change the rights on the PowerLogic Reports Folder for the SMSPR AR Operators group to allow objects to be added and modified.

1. Log in to Crystal Management Console as the Administrator account

2. Click on Folders

3. Click on PowerLogic Reports

4. Click on the rights tab. You should be on the screen below.

5. Change the access level drop down from SMS AR Operators from View On Demand to Advanced...

6. This will switch to the Advanced rights (Or Click on the Advanced link next to the drop down. Only change the following (level defaults for other items).

Explicitly Granted "Add Objects to Folder"

Explicitly Granted "Edit Objects"

Click Apply.

It may be necessary to deny the following rights but they are not required to resolve the issue:

Explicitly Deny "Modify the rights users have to objects" 

Explicitly Deny "Delete Objects"

Explicit Deny "Delete Instances"

 

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.