Browse FAQs

Is the ION 8600/8650 I/O Expander module repairable?

Published date: 11 June 2020

Issue
The I/O expander module for the ION 8600/8650 Meters is in need of repair work. 


Product Line
8600, 8650, P850EA0, P850EB0, P850EC0 or P850ED0


Enviroment
ION


Cause
The IO expander module for the ION 8600 8650 meters is in need of a repair that falls outside the scope of field repair.


Resolution
Yes the I/O expander for the ION 8600 and ION 8650 part numbers for which are P850EA0, P850EB0, P850EC0 or P850ED0 is repairable.

The repair part number is
RMAIOCARDREPAIR.

The serial number for the I/O expander will be required when requesting for repair.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.