Browse FAQs

Using ProTester DNP Master with ION meters

Published date: 11 June 2020

Issue
A user may be unable to test DNP communications on an ION meter.

Product Line
ION 7330/7350
ION 7500/7600
ION 7550/7650
ION 8600
ION8650

Environment
ProTester DNP Master

***Note: ProTester DNP Master is a product of INFO TECH, and is not supported by Schneider Electric. For information on operating/troubleshooting the software, please contact INFO TECH.***

Resolution
ProTester DNP Master is a master station simulator for DNP3.0 protocol. A trial version can be downloaded from the INFO TECH website www.infotech.pl/ .
- From the menu select: Products > Downloads > Trials for ProTester
- From the drop down select 'ProTester DNP 3.0 Master'

The following procedure demonstrates how to setup ProTester DNP Master to perform a Class 0 Poll on an ION meter.
 
Refer to DNP 3.0 and PowerLogic ION Technology technical note (70072-0105-02) to setup ION meter as DNP slave. This document has DNP architecture overview as well.
Refer to PowerLogic ION8650 DNP 3.0 device profile technical note (70022-0126-00) for description of DNP 3.0 communication protocol employed by each ION meter.
 
IONxxxx default DNP configuration:
- All DNP objects are returned in response to Class 0 Poll.
- Analog Input Objects (16-bit analog input without flag) are returned in response to Object 30, Variation 4.
- Binary Counter Objects (16-bit binary counter without flag) are returned in response to Object 20, Variation 6.
 
To Configure ProTester DNP Master to Communicate with an ION meter
  1. Select Edit > Add Line
    • Line element represents a physical connection and communication settings of the master station.
  2. Configure the ‘line’ by setting the Connection type to either Serial line or Ethernet
    • If Ethernet connection, specify the device IP address
    • If Serial line connection, specify the Port, Speed, and Parity
  1. Select Edit > Add Station
    • Station element allows to configure communication of the master station with a given slave station.
  2. Configure the ‘Station’ by assigning a station address:
  1. Highlight Sequence and select Edit > Add Frame
    • Sequence element is a container grouping other elements composing a communication procedure.
  2. Configure the frame by selecting the desired Object group, Object variation, Start point (if applicable), and End point (if applicable).
  1. Select Simulation > Start


Same frame can be modified with other functions and variations. Below are two examples:
  • Object 30, Variation 4
  • Object 20, Variation 6

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.