Browse FAQs

What is the effect on the drive rating if the vent cover on top of a drive (ATV11, ATV12, ATV31, ATV312. ATV21, ATV212, ATV61, ATV71) is removed?

Published date: 22 June 2020

Issue:
Effects of removing the vent cover on top of drives ATV11, ATV12, ATV31, ATV312. ATV21, ATV212, ATV61, ATV71.

Product Line:
Altivar ATV11, ATV12, ATV31, ATV312. ATV21, ATV212, ATV61, ATV71

Environment:
All

Cause:
Installing in a custom enclosure.

Resolution:
Removing the top cover improves air flow through the drive and may allow it to tolerate higher ambient temperatures or side by side mounting within an enclosure.
However, removing it also could allow foreign material to fall down inside the drive.
This should only be done when installed inside an enclosure.

Consult the product's Installation manual for details.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.