Browse FAQs

What is the default IP address for the G3200 gateway?

Published date: 12 June 2020

Issue  
Just got the G3200 and need the default IP address to configure it.

Product Line
G3200

Resolution
The default IP parameters are as follows:
IP: 169.254.0.10
Subnet: 255.255.0.0
Gateway: 0.0.0.0

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.