Browse FAQs

What are the different communication settings available with the Micrologic 5 and 6 in Compact NSX.

Published date: 27 February 2020

There are three types of communication settings achievable as per the hardware used with Micrologic 5 or 6 in Compact NSX.
 
  1. In config A - With the NSX cord + Micrologic 5/6. In this configuration one cannot achieve the status of the MCCB (OF, SDE, operations monitoring, motor mechanism controlled through the COM).
  2. In config B - With the NSX cord + the BSCM (Motor Mechanism COM can also be present). In this configuration one can achieve only the status of the MCCB (OF, SDE, operations monitoring, motor mechanism controlled through the COM).
  3. In config C - Combination of config A + config B. In this configuration one can get all the data in communication
 
Refer the attachment for the placement of modules in Compact NSX.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.