Browse FAQs

Is it possible to connect the Recloser Earth Leakage Device (RED) in single phase network?

Published date: 17 June 2020

Yes, it's possible to connect the Recloser Earth Leakage Device (RED) in single phase network. Refer the attached connection diagram for more details.

Note:- Connect supply to reconnection module properly and do not to leave control cable (white cable) in the air, connect them to downstream lugs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.