Browse FAQs

When attempting to import a report file into MV-90 returns "Invalid Record length in Import File”

Published date: 12 June 2020

Issue
MV90 shows an error message "Invalid Record length in Import File” or something similar when attempting to import an MV-90 Report

Product Line
ION setup 3.0
MV90

Environment
MV90 .DAT File Import

Cause
Older versions of ION setup do not have the option to choose which version of MV90 the export is intended for.

Resolution
The latest release of ION Setup has implemented an option to select the MV-90 version that you want to export for.
You are now able to choose MV-90 Xi15 or Xi30 for the MASTER.DAT file export.

Fix was implemented in ION Setup 3.0 Build 13318.02

To Download IONSETUP 3.0 Click Here

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.