Browse FAQs

What does the AA225 ION8600 flag represent?

Published date: 16 June 2020

Issue:

Eg. S8600A7C0H6C7A0A-AA225

What does the flag, AA225, do to the framework of the meter?

Product Line: 

ION8600

Environment: 

ION8600

Cause: 
 
When ordering the ION8600, what does the AA225 flag at the end of the product number represent?

Resolution:

The AA225 extender is added when there is a requirement to satisfy ERCOT 0.15% accuracy. It flags the plant to put the unit through an additional testing process to ensure the ERCOT requirement is met.

There is no change in the meter framework for this extender.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.