FAQs

Ask a Question

What cabling options are there available for the BMXDAO1605 ?

Title
What pre-made cables are available for use with the BMXDAO1605?
Issue
 
Product Line
Modicon M340
Environment
 
Cause
 
Resolution
For the BMXDAO1605, the only cabling option has a pigtail of wires on one end and a 20-way connector on the other end.  Here are the available part numbers based on the length of the cable:

BMXFTW301 -  3m
BMXFTW501 -  5m
BMXFTW1001 -  10m

 
 

Was this helpful?
What can we do to improve the information ?