Browse FAQs

How to find out how much memory was used by a SoMachine project?

Published date: 29 June 2020

Title
Memory usage for a SoMachine project
 
Issue
The customer wants to know how much memory was used by a SoMachine project
 
Product Line
M241, M251, M258, LMC058, M238, XBTGC, HMISCU, XBTGT with control
 
Environment
SoMachine 4.1
 
Cause
N/A
 
Resolution

The memory usage is displayed when, in SoMachine you go under the Logic Builder / Build /Generate code. The values will be displayed in "Message" filed

The meaning of the memory area  is:

 0 = %MW
 1= %I
 2=%Q
 3= Retain Data
 4= Application size + local variables
 5 = Persistent variables

Highest used address = available size in bytes (used or not)
Largest contiguous gap = Free available size in bytes


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.