Browse FAQs

Can I use the same line reactor from an ATV58 series that is replaced by an ATV61 with the same horsepower size and voltage?

Published date: 28 February 2020

Issue:
replaced old drive with new and needs to use the same line reactor.

Product Line:
ATV58 ATV61

Environment:
All

Cause:
Application limitations.

Resolution:
Confirm part numbers 1st  but normally the line reactors are sized based on HP, voltage and amps to it might be ok to use the existing reactor.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.