Browse FAQs

How to view CID file in XML using CET850

Published date: 17 June 2020

Issue 
Need to view CID file using XML in CET850

Product Line 
CET850
IEC61850

Resolution 
After the XML source editing is enabled (see FA228547 for details on this process), you need to highlight the CID file to edit > Click View XML Source. This will display the file in XML mode, to change back click View > Property View.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.