FAQs

Ask a Question

What drive replaces the ATV58 or ATV66 Product Line?

Issue: 
Needs a drive replacement for the ATV58 or ATV66 Product Lines.

Product Line: 
ATV58, Altivar 58, ATV66, ATV56, Altivar 66

Environment
All

Cause:
Equipment is non-functional.

Resolution:
The current replacements will be the ATV600 and ATV900 Process AC Drives, depending on application.  Use the Product Configuration tool to select the best Altivar Process Drive, to fit the application: https://www.serelays.com/flash/drives/.
 
Was this helpful?
What can we do to improve the information ?