Browse FAQs

Multiple MPPT60/80 controllers have low output.

Published date: 17 June 2020

Multiple MPPT60/80 charge controllers have lower than expected output


 In installations that use multiple XW MPPT charge controllers, they will not necessarily split the power evenly among the controllers.
If one charge controller can fufill the needs of the battery at a specific time, then the other charge controllers will regulate their power down. 

NOTE: If you are not selling to the utility and the loads are minimal, assuming the batteries are fully charged, there is nowhere else the current can flow, which is why the charge controllers would regulate their output current.
Make sure the charge controllers have the autotrack enabled and the charge cycle should be 3 stage.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.