Browse FAQs

XW MPPT60-150 shows lowlight condition but PV input is higher than battery voltage.

Published date: 17 June 2020


XW MPPT60-150 Shows low light
 
NOTE:  The PV input must be greater then Battery voltage by the following factor

Battery voltage plus a factor of 0.25 V per 12 V. For example, in a 24 V system, if the battery voltage
is 27.0 V and the PV array is producing 27.4 V, the Low Light message appears. The Low Light
message clears when the input voltage rises above the battery voltage plus a factor of 1 V per 12 V.
THIS IS NOT MEANT TO IMPLY THE ARRAY CAN BE CONFIGURED TO THE SAME VOLTAGE AS THE BATTERY. ALWAYS HIGHER.























 



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.