Browse FAQs

What are the default Modbus serial port settings for the COM'X 200?

Published date: 17 June 2020

Issue
What are the default Modbus serial port settings for the COM'X200?

Product Line
COM'X200
EBX200

Environment
COM'X200 serial communications

Cause
The default Modbus serial port settings of the COM'X200 may be unknown.

Resolution
Baud Rate: Default - 19200
Options available are  1200, 4800, 9600, 19200, 38400, 57600, and 115200


Parity: Default - Even
Options available are Odd, Even and None


Number of stop bits: Default - 1
Options available are 1 or 2


Timeout: Default - 1000ms  
Options between 100-10000ms


Terminator Resistance: Has a value of 120 Ohms and should be activated when the COM'X200 is at the end of a Modbus daisy chain.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.