Browse FAQs

What kind of cables come with the universal bluetooth interface dongle TCSWAAC13FB?

Published date: 24 June 2020

Issue
Cables included with the TCSWAAC13FB bluetooth interface dongle.

Product Line:
Altivar ATV61, ATV71

Environment:
All

Cause:
TCSWAAC13FB is the universal bluetooth adaptor uses on the Altivar ATV drives.

Resolution:
The TCSWAAC13FB comes with
Qty 1 RJ45 to RT45 cable 18 inches long
Qty 1 RJ45 to mini- DIN 18 inches long
Qty 1 C clamp
Qty 1 Install CD 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.