Browse FAQs

Is the Enercept Meter or Energy Meter bi-directional?

Published date: 23 June 2020

Issue
Is the Enercept Meter or Energy Meter capable of measuring energy flow in both directions at the same time?

Product Line
Enercept Meter (Both Basic and Enhanced Model)
Energy Meter (Both Basic model and Extended Range model)

Environment
Enercept Meter and Energy Meter capabilities

Cause
In many applications the ability to measure energy flow concurrently, in both directions, is desirable.

Resolution
The Enercept Meter and Energy Meter is not bi-directional. This means that the meter only measures energy flow either delivered OR received, but not both at the same time.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.