Browse FAQs

Troubleshooting database archive error Structureware Power Monitoring 7.0.1

Published date: 26 June 2020

Issue:
When attempting to create a manual archive in SPM 7.0.1 the user will receive the following error.

Database Manager
The following error occurred:
Object reference not set to an instance of an object.




Scheduled database backups also fail to run.

Product Line:
StruxureWare Power Monitoring Expert 7.0.x
SQL Server 2008 R2

Environment:
Database archives
Scheduled database backups

Cause:
The scheduled database backup and archive tasks require the SQL dtsrun.exe package. If this executable is not present on the machine the tasks will fail.

Resolution:
Install the SQL Server 2005 backward compatibility components to resolve the issue. The 32 and 64bit versions of the installers are attached to this article.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.