Browse FAQs

Do we offer a replacement DC choke for the ATV61/71HD90N4 drives?

Published date: 15 June 2020

Issue:
Replacement DC choke for the ATV61/71HD90N4 Drives
 

Product Line:
Altivar ATV61 and ATV71
 

Environment:
All

Cause:
DC choke needs to be replaced.
 

Resolution:
The DC choke part number is VW3A4521, available only through Schneider Field Services.  Please note that this is the choke only.  It does not include the metal box enclosure in which the choke is mounted.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.