Browse FAQs

How to configure the drive to manage brake control for horizontal applications?

Published date: 29 June 2020

Product Line:
ATV12, ATV31/312, ATV32

Environment:
Horizontal applications, no pre-torque.

Cause:
Releasing the brake as soon as the motor starts.
Engaging the brake as soon as the motor stops.

Resolution:

Wire the brake to R2A and R2C.
Configure the R2 relay as so:
[I_O-]
  "r2" = rUN
[FUN-]
  [StC-]
    "Stt" = rMP
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.