Browse FAQs

What is the effect of changing the default template name of an ION meter?

Published date: 29 June 2020

Issue
One can change the default template name of an ION meter using ION Setup in the following location:

ION Setup>Setup Assistant>Basic Setup>Nameplate Info>FAC1 Template

Highlighting the row gives following message:

NOTE: Modifying this value manually may cause some funcitons to not operate properly and should only be done by advanced users.

What might be the possible effects of changing/modifying/renaming template name in this manner?

Product Line
All ION Meters
ION Setup 3.0
ION Enterprise 6.0.x
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x

Environment
ION Setup's basic and advanced setup modes or Designer of ION Enterprise/PME/SPM by opening the meters factory module setup register.

Cause
A user may wish to give a custom name to the template.

Resolution
Changing the template string will not change the behavior of the meter itself.  It will however alter how PME and ION Setup interact with the meter.  
The template string is used to help the software decide on what screens to show the user.  If the software fails to parse the template string, then the user will have to manually decide on what diagrams to use.

If the customer wants to change the default template name they should append to the end of the name so that it can still be parsed correctly by software.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.