Browse FAQs

How to add Web Image Gadget for PME 7.2.2

Published date: 29 June 2020

Issue
When running the SQL query to add Web Image Gadget to PME 7.2.2 obtained from the Technical Publication link below:
http://download.powerlogic.schneider-electric.com/C1257BE900163231/All/A2E06D23E072D0CA85257BD6005BC879?Opendocument
The SQL query fails with the below error



Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 7.2.2 for Data Center
Power Monitoring Expert 7.2.2 for Health Care

Environment
Web Applications "Dashboards"

Cause
The SQL script from the above technical note link, checks to see if the Application Modules database is at database schema version 3. In PME 7.2.2 the database schema was changed and upgraded to version 4. 

Resolution
An updated version of the webgadget SQL query is attached.

NOTE: This SQL query has been modified to work with any version of PME 7.2.2.
NOTE: This issue has been resolved in PME 8.0 as the Web Image Gadget is installed as part of PME 8.0 installer.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.