Browse FAQs

Is there a HP rating chart for ZENL contacts?

Published date: 01 July 2020

Issue:
Identify the HP rating for ZENL contacts

Product Line:
ZENL contact blocks

Environment:
Push Buttons and Operator Interface

Resolution: 
No, ZENL contacts are pilot duty rated only and would not have a HP rating. They are rated AC-15 A600 and DC-15 R300

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.